10/5/2017 10:47 PM | |
Joined: 12/20/2016 Last visit: 10/7/2024 Posts: 13 Rating: (0) |
Thanks for the answer, Unfortunately the faceplate doesn't display any message.
|
10/5/2017 11:40 PM | |
Joined: 3/14/2008 Last visit: 10/8/2024 Posts: 2109 Rating: (941)
|
Hi, The source of the alarm must be coming from the CFC block. When you open the block properties, you can go to "Messages" on the right bottom of the screen. You can check which alarm classes are configured and what the actual message says. In the block, an Alarm_8P is called, which triggers the generation of messages. You have to determine which SIG is responsible for the alarm. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on