10/13/2008 10:59 AM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating:
|
Hi smiffy, Here are some links to manual: http://support.automation.siemens.com/WW/view/en/1137419 http://support.automation.siemens.com/WW/view/en/1188835 Here you can download ptp Parameter software http://support.automation.siemens.com/WW/view/en/27013524 When you install, there are some Example projects installed. I think you need a PtP connection in NETPRO. Best regards, Wizard |
10/14/2008 7:54 PM | |
Joined: 1/17/2007 Last visit: 7/26/2024 Posts: 1544 Rating:
|
Thanks, I have a connection setup now. However, I cannot get it to transmit or receive data. The connection (number 1001) is reported as open in Netpro, but there is no activity on the TX LED on the CP. All other LED's are off (i.e. no fault LED's). I have an RS485/RS422 module and an RS232 module. I have tried both and neither work. The status code from the BSEND FB call is 1. Find attacheda screenshot (CP441idb.zip) of the BSEND instance data block (columns are from left to right Address,Decalration,Name,Type,Initial Value,Actual Value & Comment). AttachmentCP441idb.zip (244 Downloads) |
Programming today is the race between software engineers building bigger and better idiot proof programs, and the universe producing bigger and better idiots. |
|
10/20/2008 2:06 PM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating:
|
Hi, |
10/20/2008 3:30 PM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating:
|
Hi, Is the cable correct? Who are you communicating with? Best regards, Wizard |
Follow us on