Industry Online Support
Technical Forum
11/13/2008 12:19 AM | |
Posts: 27 Rating:
|
Hello I have this MP370 on a remote site. I made a mistake and destroy the license inside. I use to be able with ALM to verify the license with the command: Edit>Connect Target System>Connect HMI Device. But I cannot any more. I always got the error Transfer error : 16842752 (0x1010000) - Connection error. That error is related to not been able to connect to the device. If I try it without any connection that is the error I got. But I know I'm connect because I open the remote manager with IEplorer and I ping the device and I can take over the control of the MP370. I connect with a dial-up and on sit ewith Ethernet. Since I can make use the Sm@rtClient, I know that my connection is OK. The ALM work fine since I can read the licenses on my computer. Why can I connect with ALM to the MP370 I use ALM 4.0, I try with 3.0 and all the patchs. Still not working Please HELP Thanks for all |
11/14/2008 8:49 AM | |
Joined: 5/8/2006 Last visit: 4/29/2024 Posts: 1085 Rating:
|
Hi, Do you use the rightinterface parameterization in the PG/PC interface? Maybe this FAQ will help you: http://support.automation.siemens.com/WW/view/de/22777582 Bye |
10/12/2011 12:55 PM | |
Joined: 4/29/2010 Last visit: 7/15/2024 Posts: 1557 Rating:
|
Hello, there is allready a helpfull FAQ about working with the ALM and a panel: What should you watch out with regard to licenses for WinCC flexible and panels? best regards. P.S. I would be better to start a new thread (as type -> Tip) than to open old threads i think. |
Follow us on