9/12/2016 1:53 PM | |
Posts: 1 Rating: (0) |
Hi! I'm not sure if this is the right place to post but didn't find another one, please can someone tell me what is the sequence of the following segment if one or both the first two conditions are not fullfilled?: Where does de program continue if "Flag machine ready" is =0 for example U "Flag machine ready" UN "HMI Flag film" L "Alarms"."W_Word 00 (Warning 09 to 16 and 01 to 08)" L 2#0001_0011_1111_1111 // No start alarms 01 to 16 UW L 2#0000_0000_0000_0000 <>I SPB MU04 L "Alarms"."W_Word 02 (Warning 25 to 32 and 17 to 24)" L 2#1111_1111_0110_0000 // No start alarms 17 to 32 UW L 2#0000_0000_0000_0000 <>I SPB MU04 Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/12/2016 2:29:13 PMNew subject after splitting |
|
Follow us on