9/25/2011 1:23 PM | |
Posts: 211 Rating: (6) |
Hi all! After installing V11 SP1 Upd2, Devices and network window DO NOT SHOW ANY Profibus component! Big bug! Any fix for it? |
9/25/2011 3:21 PM | |
Joined: 10/7/2005 Last visit: 12/24/2024 Posts: 3029 Rating: (1058) |
Hello Homeroid_BL You're in "Topology view" which is only for for displaying and configuring Ethernet Topologies, so the fix is to clickon the "Network view" tab (which will hopefully showthe Profibus devices") I hope this helps |
Cheers |
|
9/26/2011 2:16 AM | |
Joined: 10/7/2005 Last visit: 12/24/2024 Posts: 3029 Rating: (1058) |
Hello Homeroid_BL I had a "pure"TIA Portal V11 SP1 and just individual appliedUpdate 1 followed by Update 2. The results in all three "versions" are in my case consistently the same, Topology view does NOT (and need not) display any Profibus devices (it will though for example display a HMI if that HMI also has a PN port). As such I can not explain why you would have seen Profibus devices in Topology view with Update 1,but if you have, the "bug" would have been that Update 1 did display them. |
Cheers |
|
Follow us on