Industry Online Support
Technical Forum
4/23/2008 11:17 AM | |
Posts: 32 Rating: (0) |
Hi I wonder if there is a way do "bool to integer" (See picture) in S7? |
4/23/2008 12:44 PM | |
Posts: 32 Rating: (0) |
The thing i want is that if a bool is 0 then the integer becomes 0 but if the bool is 1 then the integer becomes 1. |
4/23/2008 1:14 PM | |
Posts: 487 Rating: (36) |
Hi You could In STL L 0 T MB200 A bool = 200.0 if Bool is 0 then MB200 = 0 if Bool is 1 then MB200 = 1 Eric |
4/23/2008 5:49 PM | |
Posts: 2661 Rating: (279) |
Alternately, you can scan the RLO of the BOOL input and transfer 0 or 1 to the INT output. I have created a small converter FC that does just that. Find attached the AWL source. Regards AttachmentBO_TO_INT.ZIP (417 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on