3/26/2010 4:08 PM | |
Joined: 4/24/2006 Last visit: 3/21/2025 Posts: 8904 Rating:
|
Dear ry_fern, Here is a link about OS update: how do you do an operating system update (OS update) on operator panels? You can do an OS update with or without the option 'Reset to factory settings' or Booting. In both cases, you will have to verify the port settings. You will have to do an OS update, (without Booting) then you can transfer project to panel. Best regards, Wizard |
3/26/2010 4:31 PM | |
Posts: 32 Rating:
|
Dear Wizard, So it means the OS update can be done without doing the "Bootstrap". Bootstrap happens if the panel is reset to factory settings... Thank you. |
Follow us on