1/7/2022 10:54 AM | |
Joined: 4/24/2006 Last visit: 10/14/2024 Posts: 8745 Rating: (1168)
|
Hello, When you have a PC/PG with Simatic Manager (Step 7) and the right Programming cable, it should be possible to go online and upload your PLC program. So you would have the program, however without comments and symbols. Because you do not have the original project. You can only Backup the HMI using Prosave (And restore it on the same type of panel, using Prosave) Here you can download Prosave: Or older version: ServiceTool ProSave V1.1 You will need Protool if you want to start your HMI project all over again. Best regards, Wizard |
Follow us on