5/27/2012 8:02 PM |
|
Posts: 15 Rating: (4) |
Ans here is the interface |
5/27/2012 8:02 PM | |
Posts: 15 Rating: (4) |
And here is the interface |
This contribution was helpful to1 thankful Users |
5/28/2012 5:43 PM | |
Posts: 15 Rating: (4) |
Thanks for helping me out. I knew the code could be optimized, but that doesn't really bother me at the moment. Although your suggestions sure are helpfull. I attached the program, so you can see what I've done an how things are called in the OB "main". I'm only using 1 OB. After downloading, rename the file to Test10.rar .It exeeds 3Mb as a zip file, so I made a rar file of it, but had to change the name to .zip to upload it here. If problems occur, please pm me you mail address, so I can send you the file directly. Thanks, Paul AttachmentTest10.zip (965 Downloads) |
Last edited by: PaulieTheKid at: 5/28/2012 6:30 PM |
|
5/28/2012 6:42 PM | |
Posts: 15 Rating: (4) |
This is OB "Main" |
This contribution was helpful to1 thankful Users |
Follow us on