4/8/2016 7:33 AM | |
Joined: 12/28/2015 Last visit: 3/13/2024 Posts: 13 Rating: (2) |
The interface setting snapshot is available in an attachment. |
4/8/2016 7:53 AM | |
Joined: 1/21/2016 Last visit: 4/24/2024 Posts: 43 Rating: (8) |
Hii Janak Solanki, Yes ANKURGAMIT was right please find this link for PC ADAPTOR USB driver. or following link May help you. or try this also
AttachmentSimatic_PGPC_Update.zip (1789 Downloads) |
Last edited by: Ertapu at: 4/8/2016 7:56:57 AM |
|
This contribution was helpful to2 thankful Users |
4/8/2016 11:14 AM | |
Joined: 12/28/2015 Last visit: 3/13/2024 Posts: 13 Rating: (2) |
Dear Ertapu and ANKURGAMIT I can communicate PLC with Simatic manager V5.5 via same MPI cable. So thanks for reply but my problem is still there. I have tried all possibilities that you suggested except reinstall of whole TIA portal. Suggest me if any other solution or setting is available...either or in the end i may also try the reinstall of TIA portal. Thank you. |
4/8/2016 12:21 PM | |
Joined: 12/28/2015 Last visit: 3/13/2024 Posts: 13 Rating: (2) |
Mr. ChristophD I have checked the hidden path you wrote, Up to 'Automation' folder it's correct but there is not available any 'simatic OAM' folder. The snapshot is in an attachment.
|
4/8/2016 12:42 PM | |
Joined: 12/28/2015 Last visit: 3/13/2024 Posts: 13 Rating: (2) |
Mr. ChristophD Yes, it's working fine in simatic manager and all settings are correctly displayed in PG/PC interface(control panel). Also siemens PC ADAPTOR USB A2 is working properly in TIA portal. Only MPI cable(PC ADAPTOR USB) is not working in same. |
4/8/2016 12:53 PM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
Hi, sorry but do you use different PC Adapters? or what you mean with (PC ADAPTER USB)? Regards |
Follow us on