4/28/2012 2:54 PM | |
Joined: 11/4/2011 Last visit: 12/8/2023 Posts: 253 Rating:
|
Hello sorous, this issue troubles me too. I'm even trying to make a small program that will correct old paths to moved projects. The cause could be: - changed location of the subprojects; - changed Computer name. Open multiproject in Component view and select menu View => Detailes Now look at the fields appeared: UNC path, path on 'Computer', Computer. Are the subproject and the library located at that paths? I can see two solutions: 1. Right click on every subproject and select Multiproject => Remove from Multiproject option. Then open every subproject separately as it was a single one and select the same option. Now go back to the multiproject SS1_14_MP and call Multiproject => Insert into Multiproject function, so add the subproject and the library. 2. Open folder: <MultiprojectName> \ <SubprojectName> \ s7extref \ Now you can see two files: s7envref.xml and s7pltref.xml It is possible to correct them manually. host_name - is your PC name; shared_path and local_path should be changed according to new projects paths. The second solution may be quicker if you have many projects on PC and/or in the multiproject too, because it takes much time to open every project. I guess that SIMATIC Manager is always trying to make sure that ALL of the projects in the project list are available. Good luck! |
Last edited by: TerminalBuzz at: 4/28/2012 3:11 PMLast edited by: TerminalBuzz at: 4/28/2012 3:03 PM |
|
This contribution was helpful to
5 thankful Users |
4/29/2012 8:02 AM | |
Posts: 559 Rating:
|
Dear TerminalBuzz, You are right. I have also done the same thing & the problem was solved. Dear sorous, U can also try this way. It will work. |
4/29/2012 8:18 AM | |
Posts: 13 Rating:
|
Thanks for your attention and support, It helped.
|
This contribution was helpful to
1 thankful Users |
Follow us on