11/21/2016 7:36 PM | |
Joined: 9/27/2006 Last visit: 8/17/2024 Posts: 12277 Rating:
|
Hello H. M. Suleiman; Have a look at chapter 6 "Comunication with Modicon Controllers" in ythe following WinCC Flexible manual: WinCC flexible 2008 Communication Part 2 - Siemens It describes how to configure Modbus RTU (RS-485) and Modbus TCP connections on WinCC Flexible 2008. Hope this helps, |
7/1/2017 9:47 AM | |
Posts: 7 Rating:
|
Thank you very much sir for your advise. I had checked it and when i connect my modbus device with Win CC Flexible using TCP/IP Modicon protocol, it asks me Type and addresses of Modicon PLC and there it make me fail to communicate with my Pilot PMAC 735 energy analyzer/meter. So please suggest if any other solution/driver is applicable/available so that I may connect any Modbus device without any restriction of specific device or controller. Looking for your kind advice. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/3/2017 11:40:43 AMNew subject after splitting |
|
Follow us on