8/4/2017 8:02 AM | |
Joined: 6/8/2013 Last visit: 1/29/2024 Posts: 188 Rating: (1) |
hi all i can't find fb205 and fb206 in pcs 7 libraries please help me |
8/4/2017 10:13 AM | |
Joined: 10/26/2011 Last visit: 6/12/2024 Posts: 762 Rating: (191)
|
Hello, both blocks are in the PCS_7_BASISLIBRARY_V82 or other version e. g. V80 They are called:
|
SIMATIC PCS 7 - Overview |
|
8/13/2017 12:18 PM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating: (930)
|
Hi, The blocks you describe are from the PCS7 Communication library of V5.x, which is discontinued in V6.0 or higher. If you can't use the blocks (if you are getting problems with download or communication), then you must replace them. The FR_AGSEN and FR_AGREC were used to provide a simple interface for the user. The blocks uses block calls: AG_SEND (FC5) and AG_RCV (FC6). FC5 and FC6 are available in the SIMATIC_NET_CP library under CP400/Blocks. Make sure you select CP400 rather than CP300. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on