5/25/2014 2:04 PM | |
Joined: 1/28/2009 Last visit: 10/26/2024 Posts: 6852 Rating: (1365) |
Interaction with forum is not possible currently via iPhone application(version 3.1).You can read all contribuations, you can not add your comments plus you can not download any attachments.But you can read the discussions (text) much faster!
AttachmentIMG_0703.zip (255 Downloads) |
Last edited by: hdhosseini at: 5/25/2014 2:07 PM |
|
5/26/2014 7:03 PM | |
Joined: 1/28/2009 Last visit: 10/26/2024 Posts: 6852 Rating: (1365) |
Hello Vithani, I never recommend SAFARI for serious posting in the technical forum that requires complex reasoning and checking several details in software/manual/references.Despite the convenience , you are prone to error and problem in typing that make the post less valuable .There is a sample HERE with a post via this application.I edited it again and prolonged the whole thread. Another point, due to defects in the forum's layout , it is really difficult to click the "log in" button or switch the language from English/German.When you try to zoom , case getting even worse! In brief, I think applications on portable gadgets are only suitable for casual writing in General conferences with short sentences and using some emoticons.That is all. Best regards, Hamid Hosseini |
Follow us on