1/4/2023 2:18 PM | |
Joined: 8/25/2014 Last visit: 1/25/2023 Posts: 120 Rating:
|
Hello all. I am working with a S7-1500 CPU (1511-PN) in TIA portal v15.1 and with the following regulator and motor: 6SL3210-5FB10-4UF1 (FW version 1.01) 1FL6032-2AF2x-xMA\Gx - motor with absolute encoder I cant set up the TO - Positioning axis(v4.0) to move/position the motor. I've tried to set just like it's described in the manual, but... The first thing that I can't set like in the manual is the type of telegram. One manual suggests Telegram 3, one manual Telegram 105. I have these telegrams avaliable in V-Assistant: 7,9,110,111 If I try any of these telegrams that are avaliable in the V-Assistant in the TIA portal device configuration, I cant define the Encoder. I get these errors: ,Different telegram types / addresses of setpoint Actor.Interface.AddressIn.RID and actual value Sensor[1].Interface.AddressIn.RID on the same interface are not permitted.,,,3:16:49 PM Any ideas how to configure this to make it work? Thank you in advanced. Best regards. Aleix ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/05/2023 06:35:50New subject after splitting |
|
1/4/2023 2:20 PM | |
Joined: 5/12/2006 Last visit: 3/20/2023 Posts: 21350 Rating:
|
disable basic positioning in the v90 then you should be able to select the rigth telegrams |
Follow us on