10/11/2023 6:29 PM | |
Joined: 6/7/2012 Last visit: 3/11/2024 Posts: 12 Rating: (2) |
The same problem: changing texts in Runtime settings \ Alarms has no effect. The default English texts are still displayed in Alarm Control - and the texts are linked without any separator, e.g. "incommingacknowledgedoutgoing" (or something like this). Can the alarm status texts for the Alarm Control be translated? Btw: the hint of the input field in Runtime settings \ Alarms says (e.g.): "The help topic 'CTHMIALARM@721320' (0xB01A8) is not available". Is TIA18 still an underbaked cake?[snip] Win10pro, TIA V18.0.0.1, MTP1200 Unified Comfort, indended for Czech end-users, mostly "not Unified". Thank you for any quick functional solution proposal preferably before the release of V20 . trapper66 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/12/2023 09:14:34New subject after splitting Last edited by: Jen_Moderator at: 10/12/2023 09:15:11Division of questions into separate topics. |
|
10/12/2023 9:13 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by trapper66 is split to a separate thread with the subject Can Login dialog be translated?. Best regards |
Follow us on