11/26/2010 2:12 PM | |
Joined: 10/7/2005 Last visit: 7/15/2024 Posts: 3009 Rating:
|
Hello woodpecker it seems you are asking two seemingly related yet different questions. Before we get to them let me start by saying thata DP/DP Coupler is nothing more (and nothing lesss) than a DP Slave. As such, if the I/O addressesof the DP Slave are inside the Process Image, you canof course access them from the Process Image (e.g."I" and "Q" access). As for the Process Image Partition (PIP) usage, you can do so too with a DP/DP coupler and declare the PIP for each configured I/O module inside the DP/DP coupler. Below are are couple of FAQ's that have more detail on this: Where and when do you need peripheral addressing? Use of Process Image Partitions in Organization Blocks I hopethis helps |
Cheers |
|
11/29/2010 3:32 PM | |
Posts: 2 Rating:
|
Hi fritz, Thank you very much for your reply. Your information was very useful. |
This contribution was helpful to
1 thankful Users |
Follow us on