6/23/2020 11:19 PM | |
Joined: 6/16/2020 Last visit: 11/14/2022 Posts: 9 Rating: (0) |
Hi friend, sorry. I have a logo8! Firmware v1.08.02 can be updated to a recent firmware, you will have the steps to follow and the firmware file. Thanks in advance!! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/24/2020 06:48:30New subject after splitting |
|
6/24/2020 4:33 AM | |
Joined: 12/18/2014 Last visit: 6/9/2024 Posts: 33168 Rating: (4098)
|
LOGO!s with the firmware V1.08.02 are from the first generation and their firmware can't be updatet. AttachmentVersions of 0BA8.txt (766 Downloads) |
This contribution was helpful to1 thankful Users |
12/18/2022 12:15 AM | |
Joined: 11/27/2022 Last visit: 1/4/2024 Posts: 1 Rating: (0) |
Hello ixo65, 1. If I understand correctly FS04 means FW V1.81.01 ? 2. But Model 6ED1052-1FB00-0BA8 is listed in Product innovations LOGO! 8 (FS:04), are there 6ED1052-1FB00-0BA8 running higher firmware than v1.08.0x? 3. Model 6ED1052-1FB00-0BA8 is also linked in the firmware update for LOGO! 8 for security Vulnerability CVE-2020-7593 when you search in the available downloads for the product but there is no possible update to fix this vulnerability on the LOGO running v1.08.02? 4. If I want to control my doors remotely and cannot use modbus TCP with a third party system, I could still use modbus though connected for example to something like a EWON FLexy 201 and/or create a web page using LWE?
Thank you for you help. |
12/18/2022 12:49 AM | |
Joined: 12/13/2014 Last visit: 6/9/2024 Posts: 144 Rating: (12) |
|
Last edited by: WWEE at: 12/18/2022 01:03:36Last edited by: Jen_Moderator at: 12/21/2022 05:35:17Prejudice removed. |
|
12/18/2022 5:29 AM | |
Joined: 12/18/2014 Last visit: 6/9/2024 Posts: 33168 Rating: (4098)
|
Mistakes happen at Eaton too. When the firmware V1.41 was released, the software version V7.41 came onto the market. And it's not right that Siemens doesn't do any troubleshooting. It is understandable that people are not satisfied with everything that Siemens does or does not do. Go to the Eaton forum and you will also find users there who complain about the same things you complain about at Siemens. Here's an example. |
12/18/2022 9:13 AM | |
Joined: 12/18/2014 Last visit: 6/9/2024 Posts: 33168 Rating: (4098)
|
Yes it is confusing. The LOGOs of the first and second generation had the same order numbers. LOGO! of the first generation = LOGO! 8.0. LOGO! of the second generation = LOGO! 8.1. Your LOGO! (FW V1.08.02) has no Modbus TCP/IP and the firmware cannot be upgraded. |
12/18/2022 10:23 PM | |
Joined: 12/13/2014 Last visit: 6/9/2024 Posts: 144 Rating: (12) |
|
Last edited by: Jen_Moderator at: 12/21/2022 05:36:37Prejudice removed. |
|
Follow us on