Industry Online Support
Technical Forum
6/30/2010 8:08 AM | |
Posts: 28 Rating: (0) |
Dear Sir, I am so sorry. I have just found that we also order CP1613 and Red connect. But we also have a problem which we are solving that is we use DELL computer Sever to be WinCC server. There are 2 Lan Cards. We have checked that PCI slot on this DELL does not match to PCI of CP1613. My question is can we use DELL Lan Card and install Red connect. Does it work like CP1613 with Red Connect?? Do you have any suggestion , sir? thanks Splitted from Do I need "Software redundancy" to do S7 400 redundant system?. |
Last edited by: O_Moderator at: 6/30/2010 11:33 AMnew subject after splitting Last edited by: YoonA at: 6/30/2010 8:13 AM |
|
6/30/2010 8:48 AM | |
Posts: 103 Rating: (6) |
Dear YoonA, Redconnect works only with CP1613. It will not support DELL Lan Card. You can provide the details of the type of PCI slot required for the CP1613 in PC specs. They will provide the CPU accordingly. Still if you dont have a CP1613 you can give redundacy without redconnect by running the script in the Dynamic wizard "Creat Redundant Connection".In this case your system config will be as in the attached file.Here in this system config we have a limitation in the Stahl PC tht we cant plugin CP1613 and we have still given redundancy usint the dynamic wizard script Revert back in case of any clarification. AttachmentSample systm config.pdf (298 Downloads) |
This contribution was helpful to1 thankful Users |
6/30/2010 12:28 PM | |
Posts: 28 Rating: (0) |
Thank you very much sir. |
Follow us on