6/10/2010 7:54 PM | |
Joined: 3/14/2008 Last visit: 7/25/2024 Posts: 2079 Rating:
|
Hello, My setup is as follows: PCS7 7.1 environment where a couple S7300 cpu's are connected through cp342-5 module on profibus. When i'm trying to monitor one s7300 cpu315, I often get a connection timeout.My pc is connected toa s7400 through ethernet. I access the s7300 by profibus. And after a while (few hours) I get the following error: (D063) Resource error: Trigger event occupied. Also another error showing me: (8304) No further parallel uploads possible. Too few resources. I cannot do anything with the s7300. I tried to connect trhough MPI so directlyin the s7300, but still got the same problem. My cpu number is: 6ES7315-1AF00-0AA0. I know its very old. I searched and found dat a S7315-2DP could give problems: error with few resources when not updating the firmware.I searched for mymlfb number, but cannot find any new firmware for the cpu. Do you guysknow for sure that it is my firmware? or maybe some wrong parameters..? Thanks for the help, Best regards, |
Last edited by: Oreca at: 6/10/2010 7:56 PMIf I could help you, you can use the RATE button. Thank you. |
|
6/11/2010 8:44 AM | |
Joined: 3/14/2008 Last visit: 7/25/2024 Posts: 2079 Rating:
|
Hello Umencho, youre right, small mistake in the mlfb number. But its too bad. Right now I have to do some testing and making improvements, so I really need to be able to monitor. When I'm done I only control the program from scada. Anyway, there is no way to reduce this error showing up?(any actions,configuration)I notice that I can monitor datablocks and VAR tables sometimes..without the error showing up again. Well, I notify the siemens support for this also. Thankss!! |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on