3/20/2016 9:20 AM | |
Posts: 59 Rating: (9) |
I installed and running TIA Portal V13 SP! Update7 and SIMATIC S7-PLCSIM V13.0 SP1 Update1. I cannot start simulation a S1200 devices what so ever, but with Station (S)1500 is fine. And the weirdest thing, an example or tutorial program : "SCE_EN_031-500 Analog_Values_S7-1200_R1508", that I downliaded from siemens site - whicn compile and configure with S1200 CPU/ devices, can start simulation just fine with those applications above.
please help me. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/21/2016 4:59:11 PMNew subject after splitting |
|
3/20/2016 6:31 PM | |
Posts: 8946 Rating: (999) |
S7-1200 must be Firmware v4.x or above for Simulation with TIA V13 SP1 |
3/23/2016 6:04 AM | |
Posts: 59 Rating: (9) |
How can I download that Firmaware V4.x above? |
3/23/2016 8:08 AM | |
Joined: 5/28/2008 Last visit: 9/11/2024 Posts: 1343 Rating: (141)
|
For simulation you just need to exchange the S7-1200 device in your hardware configuration. YOu need to insert S7-1200 with firmware 4.x If you have real PLC, you need new hardware with minimum FW4.0. A PLC wiht FW 1.x, 2.x or 3.x is not able to upgrade to 4.x https://support.industry.siemens.com/cs/de/en/view/106200276 |
This contribution was helpful to2 thankful Users |
Follow us on