6/9/2011 7:18 AM | |
Posts: 65 Rating: (0) |
Dear All, In case of insatalling CAS Siemens showing a procedure in this link .But while I was going to install CAS in PCS7 V7.1 SP2 ,I did not find this options in PCS7. Is there some other package separately? Please find the screen shots options which I got from the attachment. With regards, Sumanta
AttachmentCAS.zip (224 Downloads) |
6/9/2011 5:56 PM | |
Posts: 2661 Rating: (279)
|
Hi Sumanta, Please see the following FAQ: What should you watch out for when installing the Central Archive Server (CAS) in PCS7? Regards |
This contribution was helpful to1 thankful Users |
6/12/2011 8:09 AM | |
Posts: 65 Rating: (0) |
Dear Yoga Shankar, In our project there are 605 archived tags and amongst them 50 slow archived tags as it is a big system in future it may add 100 tags more .In our porject storage plus licese has purchased. As per your suggestion I think we dont need to go for CAS but storage plus may be a good option for managing archived tags and alarm and we have also storageplus license in hand. What is your opinion ? But there is some problen with storageplus configuration with redundant OS server,how can I configure storageplus with redundant OS? If you have any idea please send me. With regards, Sumanta |
Follow us on