8/3/2012 4:15 PM | |
Joined: 3/25/2008 Last visit: 2/9/2024 Posts: 57 Rating:
|
Hello, at all. I need informatios or catalog for this motor code1 PA6 186-4HF03-0AA1, please. Thanks you, enku |
8/3/2012 5:31 PM | |
Posts: 767 Rating:
|
Hello enku, For this motor 1PA6186-4HF03-0AA1 the 1PA6...motor product familywas renamed under the 1PH7... motor product familyname in 1999. Therefore almost all documentation available for any 1PA6 motor will be most readily available by using the converted name to 1PH7. In this case the equivalent part number would convert as follows: Primarily, 1PA6 changes to 1PH7 plus the digit of the "4" changes to a "2" for definition of cooling type. Also per below last digit can chagne as well, but this only defines the seals for flange and paint finish. 1PA6186-4HF03-0AA1 original motor Catalog Description COMPACT ASYNCHRONOUS MOTOR FOR CONVERTER OPERATION FORCED COOLING DEGREE OF PROTECTION IP55 4-POLE WITH 400V MOTOR VLTG WITH HTL SENSOR ROD 431 85KW,1750 RPM, 465NM TERMINAL BOX TOP CABLE ENTRY RIGHT TYPE OF CONSTRUCTION IM B 35 STANDARD DESIGN DEEP GROOVE BEARING VIBRATION SEVERITY GRADE R SHAFT/FLANGE ACCURACY GRADE R SPLINE & HALFKEY BAL. WEIGHTS AIR FLOW FROM DE TO NDE ONLY PRIMED SHAFT OUTLET IP 54 1PH7186-2HF03-0AA0equivalent renamed motor Catalog Description SIMOTICS M COMPACT INDUCTION MOTOR 74 KW, 1500 RPM, 471.1 NM, VC: 85 KW, 1750 RPM, 463.8 NM, 173 A, VC: 172 A, W/O BRAKE; WITH FAN, PG CABLE ENTRY; REL. MOTOR ENCODER HTL 1024 INCR/REV TERMINAL BOX ON TOP, CABLE ON THE RIGHT DESIGN IM B35 BEARING F. COUPLING OUTPUT, VIBRATION SEVERITY GRADE R, SHAFT A. FLANGE ACCURACY GR. N FITTED KEY + HALF-KEY BALANCING AIR FLOW FROM DRIVE END TO NON- DRIVE END IP 55, FAN IP 54, PRIMED Attached is catalog information for the 1PH7 from Configuration Manual for 400 V 3 AC line voltage in Servo Controlmode. Deputy AttachmentC:\Documents and Settings\summrl\My Documents\FY12\Reference\Forum\1PA6 to 1PH7\1PA6 to 1PH7 motor.pdf (1095 Downloads) |
This contribution was helpful to
1 thankful Users |
11/22/2017 11:04 AM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating:
|
New question published by douglaspg is split to a separate thread with the subject Catalog informations for motor model 1PA6186-4HD00-0EA3. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on