5/18/2020 1:23 PM | |
Joined: 1/27/2018 Last visit: 2/15/2024 Posts: 3 Rating:
|
dear expert do you have any idea to change the backlight of this panel tp 177A ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/02/2020 09:55:59New subject after splitting |
|
5/31/2020 9:28 AM | |
Joined: 5/28/2008 Last visit: 7/21/2024 Posts: 4514 Rating:
|
Hello, The brightness of the backlighting decreases incrementally during its operational life. You can activate automatic reduction in the screen's backlighting in screen saver settings as descriped in section 6.3.6.5 of the following manual: SIMATIC HMI HMI Device TP 177A, TP 177B, OP 177B (WinCC flexible) Hope this helps. |
Ayman Elotaify |
|
This contribution was helpful to
1 thankful Users |
6/4/2020 10:33 AM | |
Joined: 8/3/2009 Last visit: 7/19/2024 Posts: 13341 Rating:
|
Hello jacob13 what do you mean exactly?? do you want to change the Light intensity-> this is not possible you can only change the Settings for Contrast: https://support.industry.siemens.com/cs/de/en/view/21084461/3364825995 Or do you want to exchange the Backlight Hardware (Display)?? Bye Murof |
If this Information really helps, you could use the Rate function |
|
11/3/2020 9:11 AM | |
Joined: 1/27/2018 Last visit: 2/15/2024 Posts: 3 Rating:
|
Bonjour Murof je vais changé le matériel de rétroéclairage et réparer le même Merci d'avance |
Follow us on