3/21/2023 7:19 PM | |
Joined: 1/21/2013 Last visit: 6/1/2023 Posts: 1805 Rating:
|
Hi Cadej_Chudej, A comparison of the specifications of the new CPU 1510SP-1 PN (6ES7510-1DK03-0AB0) and the CPU317-2 PN/DP (6ES7317-2EK14-0AB0) shows that the processing times of the CPUs are almost identical. The total memory of the CPU 1510SP-1 PN is larger, but like all S7-1500 CPUs it is divided into program and data memory. However, for most applications this is the correct ratio. So I would say the two CPUs are pretty comparable. But it always depends on the requirements. In terms of PLC innovation, you can also think about program innovation, such as providing new features. So maybe a more powerful PLC would fit your needs better. In terms of the S7-300 family, the CPU317-2 PN/DP is characterized as a high-end CPU, while the performance class of the CPU 1510SP-1 PN is characterized as low. In general, Siemens provides a very good hardware selection software free of charge with the TIA Selection Tool. Regarding the memory card (SMC), you should be aware that a S7-1200/1500 PLC typically requires 10 times more memory than a S7-300/400. Kind regards |
Follow us on