2/16/2016 9:18 AM | |
Joined: 3/14/2008 Last visit: 9/13/2024 Posts: 2095 Rating: (936) |
Hello M_John, Are the users on the server(s) and clients the same? With the same password? |
If I could help you, you can use the RATE button. Thank you. |
|
2/16/2016 10:16 AM | |
Joined: 3/14/2008 Last visit: 9/13/2024 Posts: 2095 Rating: (936) |
Well, what settings do you have set on server and client? Maybe a print-screen....Plant-specific enabled? Did you run OS project editor on the client (assuming it's not a reference client). |
Last edited by: Oreca at: 2/16/2016 10:19:12 AMIf I could help you, you can use the RATE button. Thank you. |
|
2/16/2016 2:24 PM | |
Joined: 3/14/2008 Last visit: 9/13/2024 Posts: 2095 Rating: (936) |
Hai M_John, OS project editor is used to make settings for the user interface that the operator will use for monitoring and controlling the plant. Please find enclosed a part of the PCS7 Operator Station (V8.1). You can find the document under: https://support.industry.siemens.com/cs/document/90682677/simatic-process-control-system-pcs-7-operator-station-(v8-1)?lc=en-WW I suggest you control these steps in the document. What I meant in my previous post was a print screen of the settings at the User Administrator in WinCC Configuration Studio for the server and clients. AttachmentProcess Control System PCS7 Operator Station (V8.1).pdf (44 Downloads) |
Last edited by: Oreca at: 2/16/2016 2:24:44 PMLast edited by: Oreca at: 2/16/2016 2:25:21 PMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
2/23/2016 8:28 PM | |
Joined: 3/14/2008 Last visit: 9/13/2024 Posts: 2095 Rating: (936) |
Hello M_John, Have you made any progress? Can I help you more? Do you have some new information? Just curious. Best regards! |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on