3/28/2016 9:40 AM | |
Posts: 35 Rating: (0) |
Hello, I am analyzing the parameters of Simovert master drive which running the induction motor on close loop seed control with encoder feed back. P100 = 4 In Vector control Compendium manual sheet 350 says that kk91 connect to parameter P222 for close loop. but actually in parameter file p222 = 0 rather than 91. Can any one guide me that at which mode drive is running? and how it connect feed back value? I attache drive monitor parameter file of drive and Sheet 350 diagram. Attachmentparameter file.zip (155 Downloads) |
Follow us on