1/11/2016 4:09 AM | |
Joined: 2/20/2014 Last visit: 7/19/2024 Posts: 396 Rating:
|
Hi there, I was in the midst of testing the feature of changing user of the CMR via sms. I am having problem when i use a phone number which is of length "+60xxxxxxxxxx", 13 characters where i receive a reply sms: CHANGEUSER="xxxxxxxx","+60xxxxxxxxxx":No Success Where as if remove the country code "+6" and key "0xxxxxxxxxx", 11 characters, i get a reply sms: CHANGEUSER="xxxxxxxx","0xxxxxxxxxx":OK But when i look back in the manual, in the manual it is stated that the maximum characters permitted is 20. But when i use 13 characters, i am getting message as mentioned above. Please advise on what could be the reason for the above to happen. I have attached the one specific page of the manual which shows the maximum permitted character here for your reference. Attachmentphone number length.pdf (150 Downloads) |
1/11/2016 5:08 AM | |
Joined: 12/18/2014 Last visit: 7/22/2024 Posts: 33383 Rating:
|
I would suggest: Create a Support Request. |
This contribution was helpful to
1 thankful Users |
Follow us on