5/9/2016 9:02 PM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating:
|
Hi Nachate, Please see below my answers:
|
Last edited by: Oreca at: 5/9/2016 9:22:30 PMLast edited by: Oreca at: 5/9/2016 9:27:45 PMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
2 thankful Users |
5/9/2016 11:07 PM | |
Joined: 11/29/2011 Last visit: 6/6/2024 Posts: 1358 Rating:
|
Hi, For point3:ANY, POINTER in SCL, After you read the input bytes into the FB it is easy to address the bit you need internally. |
- What you read here, please check with manuals and your requirements. |
|
5/10/2016 7:27 AM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating:
|
Goodmorning NACHATE, Thank you for your positive comment! Well, I did not know it was PLCSim that you are using. With PLCSim, Named connections are not possible to download, so are fault-tolerant connections. You will have to change the fault-tolerant connection to a regular S7 connection in order to let it work with PLCSim. In the attachment I made a quick CFC for you with a digital input driver, an analog input driver and a digital output driver, all necessary to control a motor. You will see the signals in the red rectangle which are the inputs and outputs. There is a digital input which is the feedback of the motor, and an analog input which is displaying the actual current of the motor. To control the motor, a digital output is set. When you have assigned the inputs and outputs and the IO module you are using (Like ET200M) is released for PCS7, then during the compile with "Generate module driver" function, PCS7 will generate connections from the IO to the CFC driver blocks, which are displayed in the green rectangle. They will supply necessary information to your driver block, which you can use like a bad signal, wrong parametrization etc. I hope this is what you needed.... Cheers |
Last edited by: Oreca at: 5/10/2016 7:42:32 AMLast edited by: Oreca at: 5/10/2016 9:20:29 AMPS. Small error in the rectangle color of the digital output, uploaded again If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
2 thankful Users |
Follow us on