2/25/2013 10:21 AM | |
Joined: 5/31/2012 Last visit: 1/4/2024 Posts: 23 Rating:
|
dear sir i try to upload program for micromaster 440 drive using drive monitor with PC inverter connection kit with part no : 6SE6400-1PC00-0AA0 and because my labtop doesnot have serial port so i used USB to serial converter with inverter connection kit to connect with lab and when i try to online micromaster 440 drive the drive monitor give me short timeout and i attached photo please help best regards AttachmentDesktop.zip (613 Downloads) |
2/25/2013 5:42 PM | |
Joined: 9/27/2006 Last visit: 7/14/2024 Posts: 12268 Rating:
|
Hello Maged; See if the information in the following link can help you out: about connecting MM440 by using drive monitor and digitus usb / serial converter Hope this helps, Daniel Chartier |
7/7/2013 3:27 AM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating:
|
In addition to above, If you used AOP or starter before trying to connect by drive monitor, you also needs to check following MICROMASTER 4 (MM4): After I have used an AOP, why can I no longer go online with my frequency inverter via a BOP link with Drive Monitor? Best Regards, Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on