6/29/2017 1:54 PM | |
Joined: 9/27/2006 Last visit: 5/28/2024 Posts: 12257 Rating: (2668) |
Hello user; May I ask why you are so shy that you will not give us information on the components you want to use in your application? You won't even mention the version of hardware and software you use to program the S7-1200 CPU. Do you at least have the IODD file for the IO-Link module you want to connect to the S7-1200? You realize that it makes helping you much more difficult. So, this being a very general question on Siemens S7-1200 and IO-Link, here are some very general documents that might contain answers to your query: IO-Link System Manual V3.0 (Complete Edition) SIMATIC S7-1200 S7-1200 SM 1278 IO-Link Master firmware update V02.00.01 How do you use the Port Configuration Tool 'S7-PCT' to establish a connection to the IO-Link Master? If S7-PCT is not installed with your current version of Step 7 TIA Portal you can download it from the following link : Download S7-PCT V3.4 HF2 for IO-Link Master Hope this helps, Daniel Chartier |
Follow us on