1/8/2009 3:42 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Hello Muhammad, Can you upload here your hardware configuraion? regards |
5/4/2017 7:47 PM | |
Joined: 9/27/2006 Last visit: 6/30/2024 Posts: 12264 Rating:
|
Hello Fadi; As long as you re in the Hardware Configuration editor, could you show us a screennshot of the same window, but after activating the Online view? This si a good practice, as the HWConfig editor will identify the faulty modules with a red cross symbol. Double-clicking on each module identified with a red cross will open its diagnostic buffer. Now, the configuration seems good at first glance, it corresponds to a PPO3 (2 words PZD, 0 words PKW) configuration. What I do not understand is your mention of standard telegram 1. This is not usual with a MM440 drive. if you do not mind, i would recommend you spend a few minutes reviewing this manual: Operating Instructions: MICROMASTER PROFIBUS Optional Board It explains quit clearly the standard way of configuring a MM440 drive on Profibus how to establish communications and how to use the information in the program to start/stop the drive and change the speed setpoint. In the following link you will also find sample programs for the MM440 over profibus; MICROMASTER 4 (MM4), SINAMICS G120 (CU240S/D, DP/DP-F, PN/PN-F): Essentials for PROFIBUS and PKW-mechanism. I suggest you study the first sample, Standard load/transfer commands (English): Diagn_wd_en.zip, as it is the closest to yur basic application. Hope this helps, Daniel Chartier Edit; This FAQ collects most basic information required for communications to a MM440 drive over Profibus: MICROMASTER 4 (MM4): Setting up an MM4 with a Profibus module |
Last edited by: dchartier at: 5/4/2017 7:47:51 PMLast edited by: dchartier at: 5/4/2017 8:39:49 PM |
|
This contribution was helpful to
1 thankful Users |
Follow us on