5/11/2017 12:29 PM | |
Joined: 9/27/2006 Last visit: 9/28/2024 Posts: 12283 Rating: (2685) |
Translation from the French:
Bonjour Imma; Quelques membres du forum de Siemens parlent français, mais la majorité ne le comprend pas, car ils viennent de tous les pays . Nous avons choisi l'anglais comme langue internationale. Pour te faire comprendre de plus de participants, fais-nous la faveur de traduire tes questions en anglais lors de ta prochaine visite, svp. Les réponses te parviendront aussi en anglais. Au cas où l'anglais soit un problème, je recommande l'usage de Google Translate. Ce logiciel produit un texte anglais très compréhensible si le texte français original est grammaticalement sans faute. Hello Imma; A few members on the Siemens Forum do speak French, but the large majority do not, since they come from many different countries. We have chosen English as an international language. In order to reach more participants we would ask you to translate your questions in English the next time you come to the forum; your answers will also come in English. If English is a problem, I recommend Google Translate; his software produces a very readable English translation if the original French text was grammatically correct. Hope this helps, Daniel Chartier Now to your problem: Please tell us the distance between the 2 PLCs, and if there is any way this connection can be established through cable (copper or fiber optic?). If not, are the stations in line of site, or would you rather use a radio connection, either Ethernet radio or GPRS? Signaling and Switching via SMS with S7-1200 and CP 1242-7 GPRS V2 (Set 32)
And how much data do you need to exchange between the 2 CPUs? D. C. |
Last edited by: dchartier at: 5/11/2017 1:47:36 PMLast edited by: dchartier at: 5/11/2017 2:42:30 PMLast edited by: dchartier at: 5/11/2017 5:35:02 PMLast edited by: dchartier at: 5/11/2017 8:00:32 PM |
|
This contribution was helpful to2 thankful Users |
Follow us on