5/1/2008 6:46 PM | |
Joined: 9/28/2005 Last visit: 8/22/2023 Posts: 2957 Rating:
|
Hi, Maybe you could try to make connection parameter in WinCC Flex by hand as said in the FAQ. I mean you must configure only one CPU with Rack 0 and Slot 0 and chose Ethernet profile. After all that you can connect your OP using ethernet switch. Maybe this will work ? In that case you do not need any change connection function in your OP. The only disadvantage is that you can't see all tags form step 7 project, becouse this OP must be not connected to any network (just look at FAQ https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=22584322&caller=view, especially section "Connection setup for operator panels to the S7-400 CPU:") Unfortunally I cant test this by myself and don't know if you could do this using Ethernet. There is another option for you. You can extend your MPI/PROFIBUS line and connect OP as the last device on the line and use RS 485 repeater as decribed in FAQ. Simply you can "skip" these ET or other devices and connect OP as last device on line. That would be simpliest way. So try first option if this not work for Ethernet, use second option which 100% will be working. Good luck. Regards, |
Last edited by: Darius at: 5/1/2008 7:23 PMBest regards, |
|
7/31/2009 3:50 PM | |
Posts: 5822 Rating:
|
Hello, I am sorry, I am not the Panel specialist... and this is a Panel question but I talked to one of the specialists here and he told me that you may use this solution too. You will need the WinCC flexible 2008to run it with Ethernet too but it will work. Check this FAQ: How can you connect an operator panel directly to an H system without using repeaters? Best regards J_Bell |
8/5/2009 7:01 AM | |
Posts: 163 Rating:
|
Im unable to understand what you are asking for?SPs,HFs and build date??///// |
Follow us on