5/22/2012 11:13 PM | |
Joined: 9/27/2006 Last visit: 10/8/2024 Posts: 12284 Rating: (2685) |
Hello mayana; The Siemens A&D forum is divided in 2 sections, one in German, the other in English. Please make an effort to use English in this section of the forum, as it is the language most users share here, even though it might not be their mother tongue. As a first answer to your question on Simodrive 611 and Profibus-DP communications, please have a look at this older thread: /tf/WW/en/Posts/44633 Many members offer some good tips and links for more information on the same subject. Hope this helps, Daniel Chartier As to your second question: To see a new DP-slave in the Profibus catalog of any Profibus configurator, you need to add the gsd file (electronis data file) for that slave in the configuration software. See the online help of the TIA portal for more details. Here is a quote from the following FAQ: http://support.automation.siemens.com/WW/view/en/24210648 QUESTION: ANSWER: Here is a Downloads page from Siemens Support where you can find different downloads for the Simodrive 611U sotware releases (they include each a gsd file) based on version: http://support.automation.siemens.com/WW/view/en/10804911/133100 D.C. |
Last edited by: dchartier at: 5/23/2012 1:00 AMLast edited by: dchartier at: 5/23/2012 12:54 AMAdded link to Simodrive 611U packages |
|
4/21/2015 6:31 AM | |
Posts: 2 Rating: (0) |
Hello SIr , I want to know the purpose of the said project in the 611U-39 toolbox. Thx :) |
5/6/2015 11:41 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
|
Follow us on