7/3/2008 9:49 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
Hi, It must be possible, see COM PROFIBUS V 5.1 Not to Be Installed Under Win NT for more information. There are also new hotfixes for COM Profibus, HF1, HF2 and HF3, please install them all, they are not containing with a higher version the lower version. Hotfix 1 for COM PROFIBUS V5.1 Hot fix 2 for COM PROFIBUS V5.1 Hotfix 3 for COM PROFIBUS V5.1 It will help also if you copy the CD to the harddisk. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
2/3/2013 2:16 PM | |
Joined: 9/9/2012 Last visit: 5/18/2024 Posts: 11 Rating:
|
i also have smae problam on xp sp3 |
2/3/2013 7:16 PM | |
Joined: 9/27/2006 Last visit: 6/26/2024 Posts: 12262 Rating:
|
Hello Pradhan; If you look at the contents of the Hotfix 3 link above, here is what you will find: Installation prerequisites for Hotfix 3: System prerequisites: Windows 2000 with SP3 or SP4 This is the latest version of ComProfibus available, I reaaly doubt it can be installed on XP or later versions o Windows OS.
|
1/31/2018 9:49 PM | |
Posts: 3 Rating:
|
Boa tarde! Como consigo licença para o Comprofibus 5.1? |
1/31/2018 10:25 PM | |
Joined: 9/27/2006 Last visit: 6/26/2024 Posts: 12262 Rating:
|
Translation from the Portuguese:
Bom dia, ambev; Mais uma vez, escreva-nos em inglês quando nos visitar. Obrigado. Hello ambev, Once more, please write in English when you visit our forum. Thank you Com Profibus is a very old software, it has been discontinued for quite some time (it rums under Windows 2000, officially, some users have installed it on Win XP). If you are sure that you need this product, I recommend you open a Service Request and ask Siemens techs directly; use the link at the top of this page.The part number for COM Profibus v5.1 is 6ES5 895-6SE03.
https://support.industry.siemens.com/cs/ww/en/pv/6ES5895-6SE03/td?dl=en Unless you want to modify a Profibus network on a S5 system using a IM 308C, I think your choice of software should be validated. Explain your situation to the Siemens techs when you open a upport request, or give us more information here so we try to help you out. Hope this helps, Daniel Chartier |
Last edited by: Jen_Moderator at: 2/1/2018 12:03:34 PMInserted right link. |
|
7/4/2023 6:03 AM | |
Joined: 6/14/2019 Last visit: 10/25/2023 Posts: 10 Rating:
|
Try this:ComProfibus5.1\compbv51\Disk1\Setup.exe Good Luck! |
11/23/2023 10:33 AM | |
Joined: 12/10/2010 Last visit: 6/25/2024 Posts: 2 Rating:
|
Thx Dahema, for me this works to install it on a XP computer. |
Follow us on