7/23/2021 4:41 PM | |
Joined: 9/27/2006 Last visit: 6/14/2024 Posts: 12260 Rating: (2671) |
Hello e.bogatian; Have a look at this document, you might find it useful: How can I incorporate an AG95U DP Slave (article number: 6ES5095-8MD01) as slave in an STEP 7 project? https://support.industry.siemens.com/cs/ww/en/view/264755 Hope this helps, Daniel Chartier |
7/23/2021 4:47 PM | |
Joined: 10/29/2015 Last visit: 1/15/2024 Posts: 5 Rating: (0) |
Thanks Daniel, but document is considering S7 300 and not 1500. regards Eva |
7/23/2021 7:01 PM | |
Joined: 9/27/2006 Last visit: 6/14/2024 Posts: 12260 Rating: (2671) |
Hello e.bogatian; And, what problem does that introduce? The document shows the steps to connect a S5-95U to a Profibus master, namely a CP 342.5 in this case. In your project you want to use a CM 1542-5 as a Profibus master. The steps shown in the document are the same, the gsd file for the S5-95U is the same, the parameters for the slave are the same. If you have doubts on the setup of the CM 1542-5, look at its manual: https://support.industry.siemens.com/cs/us/en/view/109762507 The most difficult aspect of the configuration still remains: there are parameters to be set in Step 5, do you have acces to that programming software and the programming cable to connect to the S5-95U? Daniel Chartier |
Last edited by: dchartier at: 07/26/2021 02:32:35 |
|
7/26/2021 2:00 AM | |
Joined: 10/29/2015 Last visit: 1/15/2024 Posts: 5 Rating: (0) |
ok perfect, next week i will try. regards |
Follow us on