11/10/2011 1:41 PM | |
Joined: 10/11/2011 Last visit: 9/2/2022 Posts: 2 Rating: (0) |
Hi Mr Pegaia, |
Last edited by: O_Moderator at: 11/11/2011 9:02 AMnew subject after splitting from /tf/WW/en/Posts/61795#top |
|
11/11/2011 12:55 PM | |
Joined: 10/11/2011 Last visit: 9/2/2022 Posts: 2 Rating: (0) |
ok ok... I'm a newbie and I make some stupid errors. I was using one call of CE-X22for each time I need to read a variable on a Sentron... Right now that problem is solve, but like I said in my last post, I've 29 Sentron PAC to read (3x4200 + 26x3100). I'm not reading all registers on Sentrons, I've selected the most important like V, A, kW, kVAr, etc, THDu/i on PAC 4200, etc., and even so I've to call the CE-X22 4 times and the PAC [FB500] function block 12 times... In attachment is a screen shot of system resources. Any help will be most thanked. Bye Attachmentsystemresources.pdf (786 Downloads) |
This contribution was helpful to1 thankful Users |
5/18/2017 10:42 AM | |
Joined: 4/2/2015 Last visit: 6/27/2024 Posts: 1 Rating: (0) |
Hi all, I look your project... not active download link? Please send your project? Thanks
|
3/21/2018 1:13 PM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating: (169) |
New question published by AutoGen_756995 is split to a separate thread with the subject ET 200SP CPU with a bus adaptor and want to connect to an INVT HMI through Profinet. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on