5/28/2014 3:17 PM | |
Joined: 4/8/2013 Last visit: 6/30/2024 Posts: 95 Rating:
|
in /tf/WW/en/Posts/90567the same problem has occurred have you installed a "typical" package of PCS7 or didyou choose your custom Installation? and reinstallation of the machine will ( in most cases ) do you no good if you do not completely wipe the machine and start over with a fresh Windows install. in the case abovethe thread starter did not return after he dida complete machine reinstall. else, as the station manager is related to your simatic NET installation you can try to completely remove this module and reboot andafterwardstry reinstalling Simatic NET. meanwhile while you try to figure this out i would raise a SupportRequest becausethis problemsdoes not seem to have a"easy solution"according the the previous threads |
6/1/2014 4:27 PM | |
Posts: 28 Rating:
|
HELPPPPPPPPPPPPPPPPPPPPPPPPPPPPPP |
6/3/2014 12:01 AM | |
Posts: 2661 Rating:
|
Attach a screenshot of the PC Station. |
6/13/2014 4:55 PM | |
Joined: 10/26/2011 Last visit: 6/12/2024 Posts: 762 Rating:
|
Did you solve your problem? If yes, could you tell me please the solution or the reason of the behavior? Thanx |
SIMATIC PCS 7 - Overview |
|
Follow us on