10/4/2021 8:38 AM | |
Joined: 10/4/2019 Last visit: 2/20/2024 Posts: 14 Rating: (1) |
Dear Expert, I want to connect A HMI(KTP400 BASIC) to 2 WP241 module. I have prepared a project but data is not read . Here is the Gdrive link of project file. KTP400BASIC for WP241. Please help me . Thank in advance Attachment2Scale_Mbus_KTP400_Farid.zip (405 Downloads) |
Last edited by: Jen_Moderator at: 10/06/2021 12:25:26Removed link and added file as an attachment. |
|
10/4/2021 9:54 AM | |
Joined: 1/4/2007 Last visit: 5/23/2024 Posts: 1123 Rating: (174)
|
Hello fpramanik, I didn’t download your TIA project, but you have to pay attention to the following points: 1. You have to install the CSP (Communication Service Pack) on your computer: https://support.industry.siemens.com/cs/ww/en/view/109739698 Afterwards, you can select the driver „Standard Modbus TCP/IP“ in your TIA Portal project for the communication. 2. You have to use a 2nd generationKTP400 BASICpanel. A 1stgenerationKTP400 BASICpanel isn’t working. 3. On the internet, you can find an example project with 8 pieces of WP241 modules and a TP700 Comfort panel as an example for you: https://support.industry.siemens.com/cs/ww/en/view/90260674 Best regards Siwarexi |
10/6/2021 10:11 AM | |
Joined: 10/4/2019 Last visit: 2/20/2024 Posts: 14 Rating: (1) |
Dear Siwarexi, Here is the link :WP241_KPT400 [snip] 1. Yes I have download the CSP pack and installed it. I can access Modbus standard , modicon driver. 2. Please check the attached HMI part no. pic . is it a 2nd Gen. HMI? 3. I have download and check earlier that Project use VBS for CMD and Trigger tag Multiplexing. but KTP400 basic does not support VBS. You Can Support alternative. In Shared gDrive folder , I have shared 2 Project . Please check . AttachmentFiles.zip (410 Downloads) |
Last edited by: Jen_Moderator at: 10/06/2021 12:40:17Removed link and added all files as a zip file. |
|
10/8/2021 6:18 PM | |
Joined: 1/4/2007 Last visit: 5/23/2024 Posts: 1123 Rating: (174)
|
Hello fpramanik, I see no error in your project. Can you try to use my attached project for a test, please. It’s only one WP241 module, but it has to work. Maybe it helps you. Best regards Siwarexi
AttachmentMBus_WP241_Belt_KTP400_BASIC_2ND_V1.2.0_DE_ENG_FR_CN_TIAV15.1.zip (456 Downloads) |
Follow us on