4/2/2021 9:56 PM | |
Joined: 11/14/2020 Last visit: 10/30/2023 Posts: 7 Rating: (0) |
Hi! I need help to connect a PLC S7-1200 to an IOT2040. I connected the PLC directly to the IOT X2P1 (DHCP) port and the other (X1P1) port connected to the notebook. Is that correct? When I run NODE-RED on the notebook and connect the PLC directly on the same notebook everything works. But when I run the IOT so appears the following error. "Error connecting to PLC: Error: connect EHOSTUNREACH 192.168.0.50:102" I don't know what to do anymore! Thank's so much! ------------------------------------------------------------------------------------------ AttachmentSCREEN.zip (292 Downloads) |
Last edited by: Jen_Moderator at: 04/06/2021 12:24:23New subject after splitting |
|
4/3/2021 9:48 PM | |
Joined: 11/14/2020 Last visit: 10/30/2023 Posts: 7 Rating: (0) |
Hi comunity! I managed to connect the IOT to the PLC! But the error in picture stay show up! What I need to do? AttachmentPicture.zip (267 Downloads) |
Follow us on