11/13/2020 8:19 AM | |
Posts: 19 Rating:
|
HI, kindly tell me drive monitor version for window XP, as i want to connect my drive with 6SE7022-7EP60 with USB to RS232 Cable. As in my laptop i didn't have option of serial port option. later i installed Drive monitor version V5.5 in window 7 and try to connect but can not connect. I check all necessary parameters and match with software , software starts searching but did not find the drive. Regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/13/2020 12:24:27New subject after splitting |
|
11/13/2020 9:24 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello, Please do not create multiple topics for same issue/problem. Drive monitor 5.5 works with Windows7 (refer 11769381. this entry) Please check the parameters set, bus type - USS, interface select COM1, baud rate 9600, bus operation RS485 - automatic mode, in extended tab, set request retier value = 100 & request time = 40. Click OK, exit/close driev monitor. Once again open drive monitor by double clicking on icon & click on Set up an USS ONline connection, window willbe displayed, in this window click on START. Drive monitor will search for online drive & will display if it detects the drive. It this setting doesnot work, check your USB to RS232 converter cable etc. etc. HTH . |
Last edited by: PISCEAN 2010 at: 11/13/2020 09:27:14gramatical error corrected |
|
6/5/2023 11:35 AM | |
Joined: 3/25/2008 Last visit: 7/8/2024 Posts: 191 Rating:
|
hi, wiring com1 and X300 to 6SE70 and 6RA70 and then the USB to Com1 converter must be used |
Follow us on