5/8/2018 3:44 PM | |
Joined: 4/26/2018 Last visit: 9/20/2024 Posts: 2 Rating: (0) |
Hi, Marko. I've been testing your program to to connect to SQL with S7-1200 i have sucess migrating your TIA program from V13 to V14 SP1 and works wonderfull with some addins that i put (external commands, pass the address, port in a string format). But in V14 SP1 if the library stays up to V3.1 works well , but if i migrate to V4.0 or above i didn't connect i capture two shots with wireshark to see the diferences. With version >= 4.0 i never reveive the message asking login / pass. I debug your code and discover that when he is expenting the logon / pass message after the greting the RCV receives ans error (strange because the code is always the same). I need the version working with lib V4.0 because i already have one component working with that and we cannot have two diferent versions in the same project. Thanks in advance. NOTE : I have learned a lot with your posts. AttachmentCommunication SQL.zip (3789 Downloads) |
This contribution was helpful to1 thankful Users |
5/8/2018 3:45 PM | |
Joined: 4/26/2018 Last visit: 9/20/2024 Posts: 2 Rating: (0) |
Hi, See my late answer. Thanks |
5/30/2018 4:23 PM | |
Posts: 18 Rating: (0) |
Hello, what is the name of Marko Bursic's project? Thank you. |
7/15/2019 2:08 AM | |
Posts: 2 Rating: (0) |
Hello, Would you mind to share the updated project to V15? That would be very helpful! |
Follow us on