7/20/2010 11:22 AM | |
Joined: 4/29/2010 Last visit: 4/30/2024 Posts: 1557 Rating: (161)
|
Hello, sure this is possible. best regards. |
7/20/2010 11:35 AM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
Hi umair, yes you can connect the TP 177A 6" to the DP port of S7-300 CPU Connection to controller : S7-200, S7- 300/400, Win AC see section on "System interfaces" Please Have a look on the Technical Specification/Data |
Ammy |
|
7/20/2010 3:43 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Just there has limitation: PROFIBUS DP up to 1.5 Mbps. |
Follow us on