9/28/2019 1:04 AM | |
Joined: 9/27/2006 Last visit: 7/30/2024 Posts: 12272 Rating:
|
Hello sale_gr; This information applies to S7-200 CPUs, not S7-200 SMART (just in case...) What are the options for accessing an S7-200 with WinCC? https://support.industry.siemens.com/cs/us/en/view/21915573 Note that to connect with WinCC a S7-200 must use an OPC server as a bridge. So whatever your selected display, WinCC or another, PC Access should help establish up to 8 connections to different CPUs. You can purchase PC Access, a dedicated OPC server for the S7-200 family, using the part number in the screenshot below. Note the operating systems supported by PC Access. If you are using S7-200 SMART CPUs, available in the Asian market, there is an alternative: PC Access SMART: 6ES7288-8SW02-0AA0.. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 09/28/2019 01:05:32 |
|
This contribution was helpful to
1 thankful Users |
10/2/2019 11:55 AM | |
Joined: 10/19/2016 Last visit: 5/21/2024 Posts: 12 Rating:
|
Hello Daniel, thank you for the reply. It should help! [follow up questions split to: What is the best option of connecting 4 PLCs with a PC (with PC Access and WinCC)? and |
Last edited by: sale_gr at: 10/02/2019 12:42:01Last edited by: The Helping Hand at: 10/02/2019 15:52:17Reference to follow up questions. |
|
Follow us on