9/6/2023 11:50 AM | |
Joined: 8/25/2014 Last visit: 4/19/2024 Posts: 133 Rating: (1) |
Hello all. When I try to connect to a S7-1200 PLC which has a CP 1243-1 module that is connected to my clients network I get the same popup window that an IP needs to be assigned, as mentioned in this thread. If I click yes I get an error - Adding new IP address failed - Ip address allready in use, and the connection cant be established. If I click no - the connection can not be established.
If I try to ping the IP of the CP1243-1 module, it's no problem... I can ping it... Any ideas what I could do to establish the connection to the PLC. Thanks in advanced. Cheers ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/29/2023 10:39:10New subject after splitting |
|
Follow us on