6/21/2014 9:27 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Hello Slovenc Sinceyou are using a DLINK Switch, you need not show the same in hardware configuration. Just configure the Profinet ports of all the S7-1200 on a common Ethernet network. Such switches are O.K. for testing etc however I would not recommend them for permanent installation in industrial networks as these are not designed for industrial use. Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
6/22/2014 10:57 AM | |
Posts: 1064 Rating: (72) |
another hing to check is when you connect make sure that you are not set to direct connection |
Follow us on