9/26/2007 7:39 AM | |
Joined: 10/11/2006 Last visit: 8/12/2024 Posts: 5889 Rating: (802)
|
Hello adem1975, I suppose you are looking for the connection diagram for the serial cable for commissioning with DriveMonitor via serial interface? This I have attached. It is a combination cable, which can be used also for firmware downloads, if the switch is closed when powering 24V supply. It can be used for Vector and Motion control units. AttachmentKombikabel_DriveMonitor_Boot.pdf (595 Downloads) |
With best regards, |
|
Follow us on