8/23/2023 12:35 PM | |
Joined: 5/24/2016 Last visit: 5/31/2024 Posts: 325 Rating: (49)
|
Hello. As a standard 828D comes with Basic Safety Integrated. So you can have STO - Safe Torque Off SS1 - Safe Stop 1 SBC - Safe Brake Control In you're case SS1 should be what you want You can then use Termnials on the PPU on X122 - Pin 3-4 and 9-10 are described as being used for Safety Integrated. I believe one pair would be equivalent to one F-DI but you should see this in the safety integrated setup. This example is when using a TM54F modul, which is used for extended safety integrated, but the idea is the same. Here is also a link for the function manual for 828D with S120 and using Safety Integrated SINUMERIK 828D SINAMICS S120 Safety Integrated Best Regards Riddersholm |
Last edited by: Riddersholm at: 08/23/2023 12:40:17 |
|
This contribution was helpful to1 thankful Users |
8/26/2023 11:12 PM | |
Joined: 10/3/2022 Last visit: 6/2/2024 Posts: 51 Rating: (0) |
Many thanks. Thank you. |
Follow us on