1/9/2020 7:17 AM | |
Joined: 3/14/2008 Last visit: 8/10/2024 Posts: 2082 Rating:
|
Hi, Well, in this context optional is the way to go.. You want the block but for a few instances, you don't want have this block, so setting that block as optional is the solution. You may also create another CMT: One without the block, but than you won't use the concept of CMT's optimally. Do you have a problem using optional blocks? Beware that the advantage over Process Tag Types is that CMT's (types) can be synchronized with already created CM's (instances) in the project. Changes on the CM will get you warnings when you want to synchronize. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
1/9/2020 8:47 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating:
|
Hi ashadako, might be the application example Control Module (CM) Technology - Efficient Engineering with SIMATIC PCS 7 is helpful. In the application example you can find the advanced of the CMTs, how to use the CMTs with the most benfit and how to create your own CMTs. With regards |
This contribution was helpful to
1 thankful Users |
Follow us on